{}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

Is there a Raven Black spray paint available for NetShelter cabinets?

Issue:
A customer requests spray paint.

Product Line:
NetShelter SX, SV VX, WX

Environment:
All versions and serial ranges.

Cause:
Minor damage to the paint may require spray paint to cover.

Resolution:

We do not currently offer the Raven Black in spray paint, but we do have it available in a paint pen under part #690-0108-001.
Rust-Oleum has a black spray paint available that, while not a perfect match, can be used. Since it's not a perfect match the painted surface may be visible depending upon the lighting.
The Rust-Oleum part number is 7220830, Textured Black.

APC Algeria

Cela vous a-t-il été utile ?

En savoir plus
En savoir plus