{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
How to enable .NET 2.0 on Windows 8.x and 10
Issue:
PowerChute Personal Edition 3.0.2 will not install on Windows 8 or 10 because the system in missing .Net 2.0
Product Line:
PowerChute Personal Edition 3.0.2
Environment:
Windows 8.x and 10
Cause:
.Net 2.0 is not pre-installed as part of the OS
Solution:
PowerChute Personal Edition 3.0.2 will not install on Windows 8 or 10 because the system in missing .Net 2.0
Product Line:
PowerChute Personal Edition 3.0.2
Environment:
Windows 8.x and 10
Cause:
.Net 2.0 is not pre-installed as part of the OS
Solution:
You will need to install the .Net 3.5
1. Open up the control panel. (Right click start - then click control panel)
2. Verify the control panel is in Icon view
3. Go to Programs and features
4. In the left side of the window there is an option for "Turn Windows features on or off" select that.
5. You should see .NET Framework 3.5 (includes .NET 2.0 and 3.0). Check the box to the left of the .NET Framework 3.5 and click ok. Windows will proceed to install the service (downloading it from windows update if necessary).
6. After add .Net 3.5 that includes .Net 2.0 you can now install PowerChute Personal Edition 3.0.2
Vous ne trouvez pas ce que vous recherchez ?
Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.