{}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

PowerChute Network Shutdown will not communicate with or drops communication with VMware ESXi 5.5 host

Issue:
PowerChute Network Shutdown will not communicate with or drops communication with VMware ESXi 5.5 host.
In the PowerChute error.log file the error Connection to ESXi Host could not be made.java.rmi.RemoteException: VI SDK invoke exception:javax.net.ssl.SSLHandshakeException: Remote host closed connection during handshake is recorded.

Product Line:
PowerChute Network Shutdown v4.0, v4.1, v4.2

Environment:
Vmware ESXi 5.5 host

Cause:
VMware service patch

Solution:
Install the latest VMware patch ESXi550-201612001

APC Algeria

Cela vous a-t-il été utile ?