Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
Video: How to change the alarm delays on a Network Air FM unit
Issue:
This document will detail the procedure for how to change the alarm delays on a Network Air FM unit.
Product line:
FM 35-50, IR40, ACFM400, ACFM200.
Environment:
All Serial Numbers.
Cause:
Install, Configuration.
Resolution:
To change the alarm delays for temperature and humidity through the front display.
This document will detail the procedure for how to change the alarm delays on a Network Air FM unit.
Product line:
FM 35-50, IR40, ACFM400, ACFM200.
Environment:
All Serial Numbers.
Cause:
Install, Configuration.
Resolution:
To change the alarm delays for temperature and humidity through the front display.
- Press ESC key until you get to the main menu.
- Then select SETUP and then SYSTEM 1.
- Select ALARM and then select ALARM DELAYS.
- Now you have a choice of either Temperature or Humidity. Select one by using the UP or DOWN arrows.
- Then press ENTER and now you can change the delays times anywhere from 0-999 seconds.
Cela vous a-t-il été utile ?
En savoir plus
En savoir plus