{}

Nos marques

{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

Can the SRT 8 & 10 KVA be supplied by 230V, Phase to Phase?

Although the SRT 8 & 10kVA units have back-feed relays in the Live and Neutral lines and should technically work for 230V phase to phase when the UPS is configured as single phase-single feed there could be a safety issue.

This safety concerns the XLI output PDU which contains single pole breakers and only opens the one phase as compared to double pole breakers on XLT PDU breakers.  This will create a condition where the L2 (N in a single phase application)  at output PDU would have a potential of 120VAC with respect to Earth (Ground) in standby mode.
As this would create a safety hazardous condition, it is highly recommended to use the proper input wiring for this UPS as outlined in the installation or user manual to maintain the safety integrity of the UPS.  For this reason we recommend using a Transformer thus converting the 2 phase supply to a Phase and Neutral supply by bonding one leg to Earth to create an artificial Neutral.
En savoir plus
En savoir plus

Vous ne trouvez pas ce que vous recherchez ?

Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.