Consulter notre FAQ
What are the dimensions of the door handle cutout on the NetShelter SX?
Issue:
We are being asked to provide the dimensions of the door handle cutout.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Customers wishing to use a 3rd party door handle need to know the size of the door handle cutout.
Resolution:
The dimensions of the NetShelter SX door handle cutout are: (H) 150 mm x (W) 25.5 mm. (6" x 1")
We are being asked to provide the dimensions of the door handle cutout.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
Customers wishing to use a 3rd party door handle need to know the size of the door handle cutout.
Resolution:
The dimensions of the NetShelter SX door handle cutout are: (H) 150 mm x (W) 25.5 mm. (6" x 1")
Publié pour:APC Algeria
Cela vous a-t-il été utile ?
En savoir plus
Gamme :
En savoir plus
Gamme :