{}

Nos marques

Consulter notre FAQ

What is the minimum and maximum mounting depth for the SYAOPT1, and does it fit into the NetShelter 4-post rack?

Issue:
Customers may want to make sure the SYAOPT1 will mount into a particular cabinet, especially our 4-post racks.

Product Line:
Symmetra 4-Post Rack Mounting Rails SYAOPT1

Environment:
All serial ranges.

Cause:
Customers want to make sure the Symmetra 4-post rails will mount into their rack.

Resolution:

Yes, the SYAOPT1 will mount into both the NetShelter AR203A and AR204A. They are 29.42" (747mm) deep.
Minimum Mounting Depth: 27.5" (698.5mm)
Maximum Mounting Depth: 34.5" (876.3mm)

APC Algeria

Cela vous a-t-il été utile ?

En savoir plus
En savoir plus