{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
Data Center Operation | Server is running low of storage space.
Issue:
StruxureWare Operation server is running low of storage space.Product Line:
StruxureWare Data Center Operation (DCO)
Environment:
StruxureWare Data Center Operation (All Versions)
Cause:
Server does not have enough storage space to either run another backup or Operation services will not start because of backup or old data and jobs.
Resolution:
The best option would be to increase the storage size for the virtual machine hard drives. To temporally increase available space on the hard drives, Operation has a built-in service to purge old data, files, and jobs. Console into the server and run the following command:
sudo service operations purge
It is also recommended that old backups are manually moved or deleted from the /data/backup directory. To manually delete old backups navigate to /data/backup from the root directory. Then run the following command.
rm <filename>
En savoir plus
En savoir plus
Vous ne trouvez pas ce que vous recherchez ?
Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.