{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
What should I do if all or some of the fans in a NetShelter CX fail or are noisy?
Issue:
NetShelter CX fan is noisy or has failed.
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
There are several possible causes for fans to be noisy or fail.
Resolution:
Field solution - Check that the power supply unit LED is illuminated.
Check all power connections to power supply and fan tray and if necessary, change the power supply.
Field Solution - Replace fan tray.
Possible cause - Distorted or broken fan frames, bearing lubricant failed due to age or excessive temperatures or something catching the blades such as tape. etc.
Field solution - Check for anything interfering with free rotation of the blades. Check to make sure fan is seated correctly in the fan tray. If nothing is obvious, change the fan tray.
NetShelter CX fan is noisy or has failed.
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
There are several possible causes for fans to be noisy or fail.
Resolution:
All fans in the fan tray stop.
Possible cause - Power supply has failed: broken wire or loose connection.Field solution - Check that the power supply unit LED is illuminated.
Check all power connections to power supply and fan tray and if necessary, change the power supply.
Single fan failure
Possible cause - Damaged fan frame, failed bearing etc.Field Solution - Replace fan tray.
Noisy Fan
Bearing noise or ticking blades.Possible cause - Distorted or broken fan frames, bearing lubricant failed due to age or excessive temperatures or something catching the blades such as tape. etc.
Field solution - Check for anything interfering with free rotation of the blades. Check to make sure fan is seated correctly in the fan tray. If nothing is obvious, change the fan tray.
En savoir plus
En savoir plus
Vous ne trouvez pas ce que vous recherchez ?
Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.