{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
BMS AP9921X-AP9922; alarms “Battery Dry out” Sulfation Exists
Issue:
BMS AP9921X-AP9922; alarms “Battery Dry out” Sulfation Exists
Product line:
Battery Management System (BMS) AP9921X & AP9922
Environment:
All models, all serial numbers
Cause:
The response current is lower than the benchmark. Default: 30% lower than the benchmark NOTE: This alarm indicates that there is potential for a battery dry out. It does not indicate that there is a failed battery in the string.
Resolution:
Inspect the battery. Closely monitor the battery to ensure that battery dry out does not occur. • If random batteries occasionally generate Battery Dry out alarms, the Charge Current Deviation from Benchmark setting may be too close to the normal deviation range of the battery string. To reconfigure this value, see Charge Current Deviation From Benchmark • If a specific battery causes repeated alarms (especially if the alarms have increasing deviation percentages), the battery is failing. Replace the battery.
En savoir plus
Gamme :
En savoir plus
Gamme :
Vous ne trouvez pas ce que vous recherchez ?
Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.