{}

Nos marques

{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

Cannot change set point on ACPA4000

Issue:
This document explains what to do if you cannot change setpoint on an ACPA4000.

Product line:
PA4000.

Environment:
All Serial Numbers.

Cause:
How to change setpoint.

Resolution:

This document is to address a problem with the ACPA400 cool set point. If a customer cannot change the cool set point, or when they change the cool set point it reverts back to the previous set point. The reason this would happen is because the scheduling is enabled on the unit. If the scheduling is enabled it will over ride any change to the set point.

Path: Main Menu > Setup > Operating Schedule.
Program up to eight sets of environmental controls that run according to the time and day.

Scheduling:
On/Off. Select Off to use the default schedule, or on to use the programmed schedules.
En savoir plus
En savoir plus

Vous ne trouvez pas ce que vous recherchez ?

Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.