{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
Notify All Connected Users" not working in RHEL 6.3
Issue:
The "notify all connected users" function does not working in RHEL 6.3 (Red Hat Linux version 6.3)
Product Line:
PowerChute Business Edition
Environment:
OS: RHEL 6.3 X64
Build: PowerChute Business Edition 8.0.1 and 9.x OEM Basic
Cause:
Notifications are not sent to remote RHEL machines or other Windows machines in the same network.
Instead, notifications are seen only at the localhost, that is, the RHEL machine where PowerChute Business Edition is installed.
Notifications can be sent to Windows machines when this RHEL PowerChute Agent is added to a PowerChute Console.
These notifications are sent from the Console installed on Windows and not from RHEL.
Resolution:
This issue will be addressed in a future PowerChute Business Edition release.
The "notify all connected users" function does not working in RHEL 6.3 (Red Hat Linux version 6.3)
Product Line:
PowerChute Business Edition
Environment:
OS: RHEL 6.3 X64
Build: PowerChute Business Edition 8.0.1 and 9.x OEM Basic
Cause:
Notifications are not sent to remote RHEL machines or other Windows machines in the same network.
Instead, notifications are seen only at the localhost, that is, the RHEL machine where PowerChute Business Edition is installed.
Notifications can be sent to Windows machines when this RHEL PowerChute Agent is added to a PowerChute Console.
These notifications are sent from the Console installed on Windows and not from RHEL.
Resolution:
This issue will be addressed in a future PowerChute Business Edition release.
En savoir plus
Gamme :
En savoir plus
Gamme :
Vous ne trouvez pas ce que vous recherchez ?
Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.