{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
{}

Nos marques

{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ

The ESXi host running the free edition of VMware is not shutting down when commanded to by PowerChute Network Shutdown.

Issue:
VMware ESXi host, which is running the free edition of VMware, is not shutting down when commanded to by PowerChute Network Shutdown.

Product Line:
PowerChute Network Shutdown (PCNS) version 2.2.3, 2.2.4, 3.0, 3.0.1, 3.1, 4.x

Environment:
VMware ESXi versions 3.5, 4.x, 5.x, 6.x, 7.x

Cause:
The free edition of VMware ESXi provides read-only access to the API functions. Without write access to the API functions, PowerChute cannot issue a command to shut down an ESXi host.
To review a list of supported VMware ESXi versions see What VMware ESXi Licenses are support with PowerChute?

Resolution:
To make PowerChute Network Shutdown work properly you will need to purchase a license for ESXi. 

You can also find more information in Kbase Shutdown VMware ESXi 4.X, 5.X unlicensed server with PowerChute Network Shutdown

 

Vous ne trouvez pas ce que vous recherchez ?

Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.