{}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

Back-UPS CS: Runtime does not exceed 45 minutes

Article available in these languages: Espagnol

Issue:

Why won't my Back-UPS CS run longer than 45mins with a low load connected?

Product Line:

Back-UPS CS

Environment:

BK350, BK500, BK500BLK BK350EI and BK500EI

Cause:

Safety Runtime Limiter

Resolution:

The 120v and 230V International Back-UPS CS models BK350EI and BK500EI, that were made before January 1st 2004, have a max runtime limiting cap of 45 minutes. Anything made after that date will not have a runtime cap. Instead with out the shutdown software they will run until then have exhausted their battery.

APC Algeria

Cela vous a-t-il été utile ?