{}

Nos marques

{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

Alert Actions for NetBotz Version 2 and 3 Appliances

Issue:
Alert Actions for NetBotz Version 2 and 3 Appliances

Product Line:
Netbotz

Environment:
NetBotz Version 2 and 3 appliances

Cause:
The NetBotz Version 2 Appliances (320, 420, 500) support a variety of alert actions. Version 3 4xx and 5xx NetBotz also support these alerts based on configuration / connections. Some of these alert actions are only applicable if the required hardware and/or software is available. The following table defines the available alert actions and required hardware.

Resolution:

Alert ActionResultsPrerequisites
Send EmailSends an email via SMTP to one or more target recipientsnone
Send Short Message EmailSends a custom formatted email via SMTP to one or more target recipientsnone
Send SMS MessageSends an SMS text message via GSM service providerGPRS / GSM Wireless Adapter
Send SNMP V1 TrapSends an SNMP version 1 trap to configured targetsnone
Send HTTP POSTSends standard (all) alert information formatted in XML to a web server in the form of an HTTP POSTProperly configured web server and application code
Send Custom HTTP GetSends customized alert information to a web server in the form of an HTTP GETProperly configured web server and application code
Send Data to FTP ServerSends standard alert data formatted in XML to an FTP server.Properly configured FTP server
Send Custom Text File to FTP ServerSends custom alert text file to an FTP serverProperly configured FTP server
Set Switch Output StateSets the state of an device switchSupported output device such as Output Relay Pod, Power Control Pod or third party intelligent power strip
Activate Button StateActivates a push button defined on an output deviceSupported output device such as Output Relay Pod, Power Control Pod or third party intelligent power strip
Play Audio AlertPlays or speaks the text of the alertNetBotz 500, Camera Pod 120 and attached external, power speakers
Call Web Services Alert ReceiverSends customer alert information via the Web Services API to a remote systemProperly configured web server running custom application code integrated with the NetBotz Web Services API


Note: Refer to the NetBotz documentation for configuring the prerequisite hardware and software.
En savoir plus
En savoir plus

Vous ne trouvez pas ce que vous recherchez ?

Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.