{}

Nos marques

{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

How to configure NetBotz version 2 external sensors?

Issue:
Netbotz External Sensor Installation Tips

Product Line:
Netbotz

Environment:
NetBotz 2.x

Cause:
Configuration tips.

Resolution:

Adding sensors that connect to the external sensor ports require configuration before they will function. Follow these basic guidelines when adding sensors to the external sensor ports:
  • Physically connect the add-on sensor using and noting the external sensor port(s)
  • Under “Configuration” in the Advanced View, click on “Sensor Pods”. Select the appropriate Sensor Pod where you attached the sensor
  • Click “External Ports” and select the appropriate sensor and the port that it’s plugged into, then name it appropriately
  • Once that’s done, you can then select the “Sensors” button and edit the thresholds for that device accordingly
  • It’s always a good idea to test the sensors and cabling before fully deploying the solution on-site.
En savoir plus
En savoir plus

Vous ne trouvez pas ce que vous recherchez ?

Contactez notre service client local si vous avez des questions ou si vous avez besoin de plus de détails ou d'une assistance technique.