{}

Nos marques

Consulter notre FAQ

Symmetra LX - U.S. / Japan Electrical Specifications


Issue

This document describes the electrical specifications for the split-phase Symmetra LX UPS systems commonly used in North America and Japan.


Product Line

Symmetra LX


Environment

Split phase systems only (part numbers end in "P")


Cause

This information is necessary for successfully and safely deploying Symmetra LX UPS systems.


Resolution

As indicated in the Symmetra LX Electrical Installation guide, this UPS requires the following electrical specifications:



The input connection type of the LX differs from that of the existing Symmetra UPS systems. Prior to the LX, all U.S. Symmetra UPS systems required input wiring connections of L1, L1, and G only. Due to the split-phase power module design of the Symmetra LX this UPS requires the presence of a properly bonded neutral conductor. When the LX measures the input voltage it references each phase to the neutral conductor. If the neutral is not present the UPS will not operate properly. Please be aware that even if you are not intending to use 120 volts output, but only 208 volts, you still need the neutral on the input side as the design of the LX dictates this necessity.

If the Symmetra LX is not wired with a properly bonded neutral conductor, the warranty of the UPS becomes void and component replacement becomes the sole responsibility of the customer.  The input/output wiring block is clearly labeled to help electricians properly install the necessary wiring.


APC Algeria

En savoir plus
Gamme :
Symmetra
En savoir plus
Gamme :
Symmetra