{"support":{"yesButton":"Oui","noButton":"Non","feedback":{"title":"Quelles améliorations pouvons-nous apporter ?"},"submitButton":"Soumettre","successMessage":"Merci de nous avoir fait part de vos commentaires.","title":"Cela vous a-t-il été utile ?","feedbackPercentLabel":"personnes ont trouvé cela utile","captcha":{"error":"Veuillez cocher la case appropriée."}}}
Consulter notre FAQ
{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}
How do I hardwire 10kva and 20kva transformers in a 208/120 or 240/120 environment
Implementing a hardwire stepdown transformer in a 208v or 240v environment
Product Line:
Smart-UPS / Symmetra
Environment:
APTF10KT01, APTF10KW01, and APTF20KW01, All Serial Numbers
Cause:
Unbalanced UPS outputs require a stepdown transformer to power 120v loads
Resolution:
This document refers to installing the APTF10KT01, APTF10KW01, and APTF20KW01 transformers in a North American 120/240 or 120/208 environment. For installations in other regions please consult the users manual.
The wiring block outputs are as follows:
For domestic use, make sure that the Terminal Block Jumper is installed between the Ground Terminal and Terminal 8 on the output wiring block, as illustrated on page 8 of the user manual. Please also make sure that the input voltage switch is in the correct position.
The step-down transformer provides 240/120 output as 2 120v hots, a neutral, and a ground. It provides 208v output as a 120v hot, an 88v hot, and a ground. The 120v hot (terminal 7) and the 88v hot (terminal 9) are 180 degrees out of phase. You will measure 208v from terminals 7 to 9. The step-down transformer is not able to provide 2 120v hots that are 120 degrees out of phase as you would see with utility power.
Note: If your installation requires both 208v and 120v output power you will need 2 separate subpanels: a 240v/120v panel and a dedicated 208v subpanel.