{}

Consulter notre FAQ

{"searchBar":{"inputPlaceholder":"Rechercher par mot-clé ou poser une question","searchBtn":"Rechercher","error":"Veuillez saisir un mot-clé pour effectuer une recherche"}}

Network Management Card - Single Phase Symmetra SNMP Trap #77 details


Issue

Network Management Card - Single Phase Symmetra SNMP Trap #77 details

Product Line

  • UPS Network Management Card 1 - AP9617, AP9618, AP9619
  • UPS Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH


Environment
  • All serial numbers
  • All firmware versions
  • SNMPv1 or v3 traps


Cause

SNMP trap # 77 (abnormalCondition) is reserved for specific UPS failures. When trap #77 is sent, it also has a binded subtrap which gives further detail into the nature of the fault. The subtraps are specific to the UPS family type.


Resolution

Attached is a breakdown for the Symmetra single phase line of UPS (Symmetra RM, Symmetra LX, Symmetra Power Array), which uses the Network Management Card APP called 'sy'.

APC Algeria

Pièce(s) jointe(s)

Cela vous a-t-il été utile ?

En savoir plus
En savoir plus