Consultar las preguntas frecuentes

Can you change the cycle time on an InRow ACRD?

Fecha de publicación: 03 September 2020

Issue:
Can you change the cycle time on an InRow ACRD?
 
Product line:
InRow DX
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
The unit cannot operate in Lead/Lag mode under InRow operations. You will have to select HACS,RACS or Spot allowing you to access operational screen to configure Lead/Lag.

Runtime balancing can be enabled through the following path: Configure Group->Runtm Bal. When enabled the controls will shuffle primary and backup roles of units periodically to balance the system run-time of the units in the group.

Runtime balance is 72 hours.  Please note that this does not mean that the units will switch every 72 hours.  This means that the units will switch when there is 72 hours of runtime difference between the units.This is not changeable.
 

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.