Consultar las preguntas frecuentes

What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kW solution?

Fecha de publicación: 19 July 2019

 

Issue:
Symmetra PX; What is the maximum number of XR frames allowed with a Symmetra PX solution?


Product line:
Symmetra PX 20, 40, 80kW


Environment:
All models, all serial numbers
 

Cause:
The maximum number of XR frames allowed with a Symmetra PX solution is 4.



Resolution:
"This depends on the size of the Symmetra PX Main Frame.

For a Symmetra PX 20 or 40kW Frame, the maximum number permitted is 4 fully populated (Battery Frames) XR frames. This will give a runtime of 1 hr 40 mins for a 40kW load. The Battery Monitoring Card cannot handle more than this number of addresses for XR frames.

The part number for a fully populated XR frame is SYCFXR8-8. This consists of the XR frame with 8 Batteries Modules. There are 4 Battery Units in a Module this equals an XR frame with 32 Battery Units installed.

For a Symmetra PX 80kW Frame, the maximum number of additional cabinets is 3 fully populated XR frames. This would make for a total of 4 battery frames in addition to the Main UPS frame which houses the Power Modules. This will give a runtime of 35 mins for an 80kW load.

The part number for a fully populated 80Kw XR frame is SYCF8BF-8. This consists of the XR frame with 8 Batteries Modules. As there are 4 Battery Units in a Module this equals an XR frame with 32 Battery Units installed.


Note: Both battery cabinets listed above may be purchased empty (without batteries) by omitting the ""-8"" at the end of the part number."



 

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.