Consultar las preguntas frecuentes

IP Installer Utility for APC KVMXXXX Digital IP KVM Switches

Fecha de publicación: 28 July 2014


Issue

IP Installer provided for user download in order to configure/modify TCP/IP settings for APC KVMXXXX Digital IP KVM switches


Product Line
  • Rack Accessories - KVM Switches
    • KVM1116P
    • KVM2116P
    • KVM2132P
       

Environment

  • All serial numbers
  • KVMs connected via network


Cause

One option for users to assign TCP/IP settings is to use the attached IP Installer .exe on Windows systems to locate APC KVMXXXX Digital IP KVM Switches via the network. This tool requires that the "IP Installer" setting in Device Management menu is set to Enabled. If the setting is set to View, the user can search and identify the KVM but not modify TCP/IP settings. If the setting is set to Disabled, the KVM switch will not be discovered by the utility.


Resolution

Download the attached .exe file in order to utilize the tool. Alternatively, a user can connect a keyboard, monitor, and mouse to log in and configure the KVM switch as well.

¿Ha sido útil?

¿Qué podemos hacer para mejorar la información?

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.