Consultar las preguntas frecuentes



Batteries; Is it OK to replace the internal batteries or use refurbished modular battery modules?
... PX1 20 - 80 kva , Symmetra PX2 100 kva , Symmetra PX 250-500 kva , SUVT, ... , ais3000, Galaxy VM
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... user is unable to access their APC ... ... are two parts to this issue, ... Card product configured for SSL (HTTPS ... ... browser products due to numerous security vulnerabilities ... One such vulnerability is ... ... will fall back to sslv3.0 ... , be vulnerable to POODLE. ... ) is configured for HTTPS. ... ) is configured for HTTPS. ... Card is configured for HTTPS. ... or anything referring to invalid key size ... may be due to a separate issue ... ... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but are not limited to ): Metered ...
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from total power off to normal on- ... Galaxy 5000, Galaxy 5500 For various reasons, the Galaxy 5000 may be ... ... guide illustrates how to restore it to normal operation. ... This is not for commissioning a new UPS . ... of a new UPS must be performed ... trained and qualified service representative. How to restore the Galaxy 5000 UPS from total power off to normal operation. ... This procedure is for a single UPS without an external ... Step 1 : Set the input Q 1 switch to On
AOS v6.3.2/sy3p APP v6.3.2 UPS Network Management Card 2 (NMC2) ap9630/AP9631 UPS Compatibility
... v6.3.2 will provide support for Symmetra PX 20, 40, 80 kVA models only (especially to help address ...
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
How to take the Single Galaxy 5000 UPS from normal operation to total power off ... Galaxy 5000, Galaxy 5500 Due to site maintenance, ... request come in for assistance with Powering Down the Galaxy 5000 UPS The instructions to power down the UPS are available on ... ... This procedure is for a single UPS with an external ... Step 1 : Touch any ... on the display to wake it up ... ... 3: Scroll to “Maintenance” ... “Stop the UPS Step 5 : Press the ... gray) button for 3 seconds to transfer the load to the Static Bypass ...
Smart-UPS VT-Galaxy 3500; Bypass Not Available Input Freq/Volt Out Of Range, Output: Inverter sync. to bypass alarms
Smart- UPS VT- Galaxy 3500; Bypass ... Smart- UPS VT- Galaxy 3500-ais3000 ... of acceptable range for bypass operation. ... occurs when the UPS is online, ... , the UPS should not allow you to command the UPS to bypass. If the UPS allows you to enter Static Bypass ... alarms are displayed for 20> seconds ... the input voltage to provide acceptable voltage ... ... Input frequency range for the PFC is ... ... window, the UPS should be in ... For 60 Hz systems: 60 HZ +/- 0, 1 %
​Information for Noise level of UPS Galaxy 5000 NAM
Information for Noise level of UPS Galaxy 5000 NAM ... Galaxy 5000 NAM ... Galaxy 5000 40kva, 50kva,60kva, 80kva, 100kva and 130kva ... Customer needs UPS room noise level with Galaxy 5000. ... for Galaxy 5000. ... Measured according to ISO 3746 (NFS 31 027). UPS acoustic pressure level for linear loads are indicated below. UPS rating ( kVA ) 40/50/ 60 /80kva 100/130kva Noise level on a normal floor (dBA) with an RL load at 3 feet 65 63
MGE STS, Galaxy 3000, 4000, 5000 and Galaxy PW; Wiring information for egx100 to any 66061-supported products
Wiring information for egx100 to any 66061- ... ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW ... – STS, Galaxy 3000, 4000, 5000 and Galaxy PW Wiring information for egx100 to any 66061- ... ... card is configured for 9600, 8 , N and 1 . Slave address is 1 and wiring is ... ... This assumes only one 66061 card or UPS or STS is connected to the enclosure but ... ... card is RS232 for configuration. ... must be wired to . ... IP address needs to be configured at ... One is down ( ...
Video: How to take the Galaxy 5000 UPS from normal operation to total power off?
... Down the MGE Galaxy 5000 UPS Galaxy 5000, Galaxy 5500 Due to site maintenance, ... request come in for assistance with Powering Down the Galaxy 5000 UPS The instructions to power down the UPS are available on ... ... This procedure is for a single UPS without an external ... Step 1 : Touch any ... on the display to wake it up ... ... 3: Scroll to “Maintenance” ... “Stop the UPS Step 5 : Press the ... gray) button for 3 seconds to transfer the load to the Static Bypass ... ... protected by the UPS .
Video: How to place Galaxy VM UPS into Maintenance Bypass
Cause: The UPS must be transitioned into maintenance bypass mode for certain types of service or other maintenance to the system.


Resultados 1 - 10 de 70

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.