Consultar las preguntas frecuentes



Batteries; Is it OK to replace the internal batteries or use refurbished modular battery modules?
... PX1 20 - 80 kva , Symmetra PX2 100 kva , Symmetra PX 250- 500 kva , SUVT, ... , ais3000, Galaxy VM
How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel
Issue: How to take the Single Galaxy 5000 UPS from normal operation to total power off using an external Maintenance Bypass Panel.
Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS?
Issue: Does the NTP need to be configured on the Galaxy VS internal NMC and the optional AP9644 NMC for all parallel or single Galaxy VS
Where can I find Hazardous Materials Quantities for C&D Technologies batteries used in MGE EPS, Galaxy and galaxy PW products?
EPS 6000, EPS 7000 , EPS 8000, Galaxy PW, Galaxy 5000, Galaxy 4000 ... G5K 40kva with one string of UPS12-490fr will have 36 batteries, 100% run time 61 min.
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM.
Default password of 1234 does not work on the Display of new Galax VX or Galaxy VM. ... Galaxy VX, Galaxy VM ... To conform to California law SB 327 which requires the ender user to change the password when first logging into a network device. The display of the Galaxy VX and VM is part of the NMC and has been disabled. ... Serial port setting: for 9600 bps, 8 data bits, no parity, 1 stop bit, and no flow control.
Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Transitioning the Galaxy 5000 UPS from ... Galaxy 5000, Galaxy 5500 ... For various reasons, the Galaxy 5000 may be in a totally off state. ... How to restore the Galaxy 5000 UPS from total power off to normal operation. This procedure is for a single UPS without an external bypass panel. ... Step 1 : Set the input Q 1 switch to On Step 2: Wait until the end of the UPS initialization with PFC start -up. ... Step 4: Choose “ Start the UPS” ... Step 9: Press the Green “Inverter Start Button”
Modbus Installation and Troubleshooting for AP9635/AP9635CH Network Management Card 2 (NMC2)
... support Modbus TCP or Modbus RTU with AP9635/AP9635CH ( Galaxy VM, Galaxy 300/ 7000 , Galaxy 5000/5500, etc ...
What is the expected life of my APC UPS battery?
... battery life, PX1, Smart-Ups VT, Galaxy 3500, PX2, PX 250- 500 , Galaxy , PW, Comet ...


Resultados 1 - 10 de 60

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.