Consultar las preguntas frecuentes



UPS Network Management Card replace battery date year is missing or incorrect
... /time on a Network Management Card 1 and 2 (v3. X . X , 5 . X . X firmware) via ...
NetBotz 750 | Resetting a Lost Root Account Password
NetBotz version 5 NetBotz v 5 . X Reset a Lost Root Account ... 1 ) Connect a USB- A to Micro USB ... NetBotz appliance and a USB port on ... ... 2) Open a serial connection on ... ... Data Bits: 8 ... Stop Bits: 1 ... specified in step 1 . ... do not press a key within five seconds after you ... 5 ) Enter the ... ... do not press a key within 5 seconds after you ... 8 ) Enter the following three commands: ... NOTE: If you do not complete steps 7 and 8 , the root password will be reset every time the appliance restarts.
Smart-UPS SRC 5k, 6k, 8k and 10 KVA FAQ
Both the UPSs share the load equally but if one fails (either through developing a fault or being taken out of service for maintenance ...
Troubleshooting steps to perform when "Please check that the USB cable between your battery backup and PC is properly connected" message or "Unknown Device" appears after a reboot of your computer.
... BACK-UPS XS , BACK- ... 1 . Ensure that ... 5 . Cycle power ... 8 . Ensure that ... ... is plugged into a USB hub try ... ... and retry steps 1 - 8 . If so, there are a few parameters of your PCs BIOS that need to be changed in order for your PC to recognize the USB device as an APC UPS after each boot. ... Note: An APC representative cannot make changes or assist customers in making changes to the BIOS, as it is a liability to APC. The BIOS of your PC is both manufacturer and model specific.
How can I adjust the number of battery packs on a Smart-UPS XL?
All models , All Serial ... : Models that begin with ... are not XL models , even though ... ... -UPS XL models are not designed ... ... -UPS XL models are not designed ... ... runtime calculations which a Smart-UPS ... 1 . Using Hyperterminal ... ... battery packs via a Hyperterminal session: 1 . First, ... ... asked to choose a name and select ... If a message appears which ... .must install a ... 2400 baud, 8 data bits, 1 stop bit, ... 5 . Click on ... a . Type " ... ( A new unit will ... ... "" Adds a battery pack
How is the rackmount U-space of a NetShelter cabinet or rack identified?
Vertical Hole spacing must follow a pattern of 5 / 8 ""- 5 / 8 ""- 1 /2"" ...
General Receptacle Wiring Practices
For 120 volt applications, any one of the hot phase ... copper-colored terminal on a suitable NEMA X 5 -XX receptacle.
How do I upgrade the firmware of an XU1K3LLXXRCC using a USB Thumb Drive?
... an XU1K3LLXXRCC using a USB Thumb Drive ... ... firmware upgrades via a USB Thumb Drive ... This is a method unsupported by ... ... this firmware via a Network Management Card ... During the upgrade process the UPS will not be able to provide battery backup in the event of a Power Outage ... Step 1 Copy the xul1017ups_02-6.enc image to a USB Thumb Drive ... After 1 minute, the USB Device menu will appear. ... Step 5 ... Display automatically pop ups with “Receiving Firmware Image X % Completed” Step 8 ... Display automatically pop ups with “Installing Firmware X % Do Not Power Off”
Video: Data Center Expert | Backing up to a Windows Share
... Process for creating a Windows share backup ... ... version 6. X to 7. X ) ... be performed on a regular basis. Creating a Windows Share Performing a Backup within DCE Creating a Windows Share ... versions may prevent a windows share from ... 1 ) Create a folder on the ... 5 ) Set the ... 8 ) Ensure that ... ... user as step 5 ). Performing a Backup within DCE 1 ) Open the ... ... Steps 3 & 5 ) ... computer is on a domain, enter ... ... Subdirectory: If a subdirectory was created ... 5 ) Select Test ...
Data Center Expert | How do I restore to defaults and restore a backup?
... Process for restoring a StruxureWare Data Center ... ... to defaults and a backup to be ... ... usually done per a request from Data ... Restoring a Data Center Expert ... Restoring a Data Center Expert ... Restoring a backup on a Data Center Expert ... Restoring a Data Center Expert ... 1 ) Download and ... ... Instructions for deploying a virtual appliance can ... ... let VMWare choose a MAC address and ... Restoring a Backup on a Data Center Expert ... Restoring a Data Center Expert ... 1 ) Contact technical ... ... 2) Create a bootable USB restore ... ... you are restoring a version prior to ... .4. X the maximum size ...


Resultados 1 - 10 de 97

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.