Consultar las preguntas frecuentes



Input Circuit Breaker Requirements for Symmetra PX 20/40/80 kw
This document describes the required input over current protection (circuit breaker) required when installing a Symmetra PX ... Input Circuit Breaker Requirements for Symmetra PX 20/40/80 kw ... Symmetra PX 40 ... 80a 480vac ( PDU w/ Step Down Transformer required) 60a 600vac ( PDU w/ Step Down Transformer required) Symmetra PX 80 ... 150a 480vac ( PDU w/ Step Down Transformer required) 125A 600vac ( PDU w/ Step Down Transformer required) ... (APC Symmetra PX Frame Installation Deviation and Selection of Input Circuit Breaker Ratings)
acdc1010 Hot Aisle Containment Rack Expansion Bundle Kit Installation (Manual)
... describes how to install an acdc1010 Hot ... Install , A Rack ... Ceiling panel assemblies come with Lexan ... ... when removing/ installing side panels from a PDU , UPS, or XR Battery Cabinet. the PDU , UPS, or XR Battery Cabinet while ... ... operation while the PDU , UPS, or XR Battery Cabinet is ... ... electricity to the PDU , UPS, or XR Battery Cabinet, ... ... working on the PDU , UPS, or XR Battery Cabinet. ... required to correctly install your Rack Expansion ... ... the door frame assembly from the equipment ...
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
NOTE: If you have an AP9635 installed in a Symmetra PX 250/500, you have a Network Management Card 2 but MUST
What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kw solution?
There are 4 Battery Units in a Module this equals an XR frame with 32 Battery Units installed .
AP8XXX Rack PDU 2G "NMC CAN Bus Off" Error
For units manufactured later than December, 2012, you may find a CAN bus terminator pre- installed in one of these ports.
Symmetra PX1-PX2; What happens when PX1, PX2 and 250/500k PX is EPO'd
... 250/500k PX is EPO'd Symmetra PX ... how the Symmetra PX reacts to the ... PX : ... If the EPO circuit in the Symmetra PX is activated the System Enable Switch turns to the off position, the DC Breaker in the Main Frame or in the XR Frame (80kw units only) also switches to off. Mains feed CB will be tripped on ISX PDU . There is no power on the output of the XR Battery Frames or on the output of the Symmetra PX UPS. ... PX : ... Only the Battery CBs on XR frames will be tripped. ... PX :
Rack PDU 2G (AP8XXX) Network Port Sharing Information
... of AP8XXX Rack PDU models AP8XXX Rack PDU series only ... on the Rack PDU front panel. ... the same Rack PDU firmware revision, ... ... AP89XX series Rack PDU was manufactured prior ... AP89XX series Rack PDU was manufactured after ... been pre- installed for you in ... ... your group is ready , you can ... ... terminator pre- installed . ... a pre- installed low profile terminator ... ... for the Rack PDU group. ... as a Rack PDU that is connected ... of a Rack PDU group. Set up network functionality for this Host Rack PDU as specified in ...
Can I install multiple APC SmartSlotAccessory Cards in one UPS?
Can I install multiple APC SmartSlotAccessory Cards in one UPS? ... Symmetra PX (excluding PX 250/500) ... If a user requires multiple SmartSlot cards to be installed , this articles what is available to accomplish that and any associated requirements. ... APC does manufacture a SmartSlot Expansion Chassis for multiple APC SlotSlot Accessory cards, though this chassis is considered a legacy product. ... Please see the following link for installing multiple SmartSlot accessories in a supported UPS system:
Can I plug my APC Rack-Mount Power Distribution Unit (Rack PDU) into a feed receptacle located in the under floor plenum? (Also applicable to Configurable & Modular Power Distribution)
645.5 Supply Circuits and Interconnecting Cables (2) Cord set assembly , where run on the surface of the floor, shall be protected against physical damage. ... (1) The raised floor is of suitable construction , and the area under the floor is accessible. ... These supply conductors shall be installed in accordance with the requirements of 300.11.
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
px2 Symmetra PX 48/ 96 /100/160 kVA embedded UPS brain AOS v3.9.0 and higher Yes ... rpdu AP7XXX series Rack PDU (ex. ... pxhid AP9361 Rack Access PX -HID AOS v3.9.0 and higher Yes ... rpdu2g AP8XXX series Rack PDU 2G (ex. ... sypx Symmetra PX 250/500 kVA (w/AP9635 only) AOS v6.3.2 and higher Yes (via your local 3-phase technical support team) sy3p Symmetra PX 20/40/80 kVA


Resultados 1 - 10 de 77

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.