Consultar las preguntas frecuentes



How to configure the SRC 5,6,8 & 10 KVA UPS Models External Battery Packs using the LCD display
In order to setup the external battery packs, please key in as (Ah of battery ) x (total number of batteries ) ...
How can I adjust the number of battery packs on a Smart-UPS XL?
... how many external batteries are connected so ... ... can use external batteries . ... and have Smart Batteries . battery packs. battery packs. batteries effects the runtime ... ... is running on battery power. ... number of external batteries . external battery packs ... the number of battery packs via a ... the UPS service must be stopped ... ... ..must install a ... 2400 baud, 8 data bits, ... 5 . Click on ... ... " Adds a battery pack ... number of external battery packs ... " Subtracts a battery pack ... number of external battery packs ... the number of battery packs via a ...
Troubleshooting steps to perform when "Please check that the USB cable between your battery backup and PC is properly connected" message or "Unknown Device" appears after a reboot of your computer.
... cable between your battery backup and PC ... ... BACK-UPS XS , BACK- ... ... the following APC Battery Back-UPS ... ... drivers can be installed from your corresponding ... 5 . Cycle power ... 8 . Ensure that ... ... see listings as Batteries and Human Interface ... ... drivers are already installed . ... steps 1- 8 . 11. Reboot your PC. After reboot, did your PC recognize the UPS or are you still receiving the initial message of ""Please check that the USB cable between your battery backup and PC is properly connected""?
Video: How do I upgrade the firmware on an APC Network Management Card (NMC) or NMC embedded device (Rack PDU, etc)?
... Management Card is installed in to be ... ... device from v 5 . X . X to v6. X . X , please review ... ... have an AP9635 installed in a Symmetra ... ... Network Management Card installed in. ... Network Management Card installed in a UPS ... Silcon * ... v3. X . X Firmware for Smart ... /AP9617/ 8 /9 installed ... v6. X . X Firmware for Smart ... ... firmware 3. X and Network Management ... AP9631 use version 5 . X or 6. X firmware.
Why does Symmetra LX see only half of my installed battery modules?
The bottom intelligence module monitors battery bays 1, 3, 5 , 7, ... , 6, 8 , 10, &12.
How do I upgrade the firmware of an XU1K3LLXXRCC using a USB Thumb Drive?
During the upgrade process the UPS will not be able to provide battery backup in the event of a Power Outage ... Step 5 Scroll down and select “ Install UPS Firmware” ... Display automatically pop ups with “Receiving Firmware Image X % Completed” Step 8 ... Display automatically pop ups with “ Installing Firmware X % Do Not Power Off”
PowerChute Network Shutdown continually shuts down the ESXi host following On Battery Shutdown and UPS turn off when A/C power has been restored in Advanced UPS Configuration.
VMware ESXi versions 4. x , and 5 . x ... PowerChute is installed on a physical Windows machine and configured for Advanced UPS Configuration. ... Upgrade to PCNS version 4. x
How to enable .NET 2.0 on Windows 8.x and 10
Windows 8 . x and 10 ... .Net 2.0 is not pre- installed as part of the OS ... You will need to install the .Net 3.5 ... 5 . You should see .NET Framework 3.5 (includes .NET ... Framework 3.5 and click ok. Windows will proceed to install the service (downloading it from windows update if necessary). ... 2.0 you can now install PowerChute Personal Edition 3.0.2
Video: Back-UPS XS/RS "G" Battery Installation and Replacement
Cause: Battery installation for replacement or initial configuration.
Symmetra LX Battery Module Information Missing within v6.X.X Network Management Card Firmware Web Interface
Users with an ap9630 or AP9631 UPS Network Management Card 2 v6. X . X installed in a Symmetra LX UPS may notice ...


Resultados 1 - 10 de 82

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.