Consultar las preguntas frecuentes



What materials are used in the main structure and acoustic foam lining of the NetShelter CX?
... a combination of Medium Density Fibre Board (MDF) and High Pressure Laminate ( HPL ) on its top and MDF on its plinth ...
How to navigate through an Network Air FM unit display
... %) or high efficiency (65 ... Suction Pressure Compensation. ... if the suction pressure gets too high . ... FM in a high -density application Max ... —Use the maximum value reported by ... ... to maintain head pressure in DX Systems ... Clear all of the output mappings back to their default setting. ... Set the nominal coil differential pressure . ... Displays the coil differential pressure . The coil differential pressure changes as the blower frequency is adjusted. ... pressure for the FM DX Precision Air Conditioner. ... Set the nominal coil differential pressure . ... Displays the coil differential pressure . The coil differential pressure changes as the blower frequency is adjusted.
How many networking cables can a NetShelter CX accommodate?
(The 38U cabinet has two cable ports, one at the top rear and one at the bottom rear ).
What filter is being used for your InRow 300mm?
Maximum Height : 4.80 inches (122 mm)
How to replace a NetworkAIR FM Series Filter Replacement
Net Weight 2.27 kg 5lbs Maximum Height
Recommendations for protecting a laser printer
Even small Laser Printers can have very high maximum power draws, due to the nature of the technology.
Does the ACSC automatically restart after a high head pressure alarm?
Issue: Does the ACSC automatically restart after a high head pressure alarm?
How does the high head pressure protection feature work on the ACSC?
Issue: How does the high head pressure protection feature work?
What is the maximum allowable pressure for the water side of an acrd200?
Issue: This document details the maximum allowable pressure for the water side of an acrd200?
Please explain Suction Pressure Compensation for the NetworkAIR FM.
This feature is designed as a safeguard against high suction pressure conditions when the FM is used in a high return air temperature environment.


Resultados 1 - 10 de 85

¿No encuentras lo que buscas?

Ponte en contacto con nuestro equipo de atención al cliente para obtener información sobre asistencia técnica, asistencia para quejas, etc.