Configuring the Native Serial Shutdown Support in Windows 2000, XP, or 2003
Step # 1 : ... If the UPS tab is not present, uninstall all APC Software packages including PowerChute Plus and PowerChute Business Edition and reboot the machine. ... The UPS service is currently stopped. The UPS service , by default, is set to start manually. Once configured, the UPS service will start on bootup. ... Note 1 : ... 1 Stop Bit ... To save the new settings and start the UPS service , click Apply. ... UPS, you will also receive information such as Runtime, Battery Capacity and battery condition.