Our Brands

APC USB Wi-Fi Device in UPS

New! Wireless USB Wi-Fi Device

The APC USB Wi-Fi Device enables wireless access to your Network Management Card 3 enabling remote monitoring and control of your UPS by connecting it directly to the network providing:

• Flexible, simple installation
• Removal of traditional cabling
• Easy updates to the wireless network

 

EcoStruxure IT Integration

APC Network Management Card enables access to EcoStruxure IT which provides global visibility of your critical infrastructure and alarm notification in the event of an issue.
 

Security Enhancements

APC Network Management Card has modified its security features to reflect the new internet connected device requirements.

New legislation around internet connected devices require stricter security features. The increased security modifications are present in APC Network Management Card 2 firmware update v6.8.0 and above.

Enhanced Security, What’s Changed?

 

Secured Interfaces

Only HTTPS, SSH and the local console port are enabled. Some interfaces require creation of associated authentication credentials before they can be enabled.
 

Introducing the Next Generation

Refreshed with latest technology and new features the Network Management Card 3 is here and is more powerful than ever

Next Generation Features

 

Enhanced security

New advanced security features to keep your sensitive data secure with newest compliance offerings
 

High-performance

Featuring a new processor and 1Gigabit ethernet connection
 

Extensive storage

Extended memory space to accommodate increased event and data log storage
APC Network Management Card 3 provides an easy-to-use, reliable remote management solution.
  • Micro USB based console
  • 100x event log and data log memory storage
  • Pre-loaded language support
  • SMTP email authentication with latest standards

What is the End-of-Life support of Network Management Card 2?

The 2nd generation network management card end of sales date is December 2020. There is an additional year of support for firmware updates to reflect any further security changes.
For more information regarding product support read the End-of-Life policy document.

Which Network Management Card is compatible with my device?
The compatibility chart breaks down the pairing between UPS models and Network Management Card.

Learn more

Depending on your UPS model, the Network Management Card is embedded or pre-installed with purchase. Ensure your model includes the upgraded card by understanding the transition timeline.

Get the transition details

How do I know which card is installed in my device?

Upon login, the top banner on the interface specifically states which card is installed. Smart-UPS with a bundled network management card packaging also explicitly calls out which card is present.

Upgrade Now

Upgrade to the latest version Network Management Card with new security features, improved functionality and increased ease of use

Q&A

Understand the transition details and the Network Management Card 3’s features in greater detail by reading the frequently asked questions.

Questions?

If you have more questions, please contact our customer support
Your browser is out of date and has known security issues. It also may not display all features of this website or other websites. Please upgrade your browser to access all of the features of this website. Latest version for Google Chrome, Mozilla Firefox or Microsoft Edge is recommended for optimal functionality.