Video: How to take the Galaxy 5000 UPS from total power off to normal operation.
Published date:
07 May 2018
Issue:
Transitioning the Galaxy 5000 UPS from total power off to normal on-line operation.
Product line:
Galaxy 5000, Galaxy 5500
Environment:
All models, all serial numbers
Cause:
For various reasons, the Galaxy 5000 may be in a totally off state. This guide illustrates how to restore it to normal operation.
Note: This is not for commissioning a new UPS. The commissioning of a new UPS must be performed by a Schneider Electric trained and qualified service representative.
Resolution:
How to restore the Galaxy 5000 UPS from total power off to normal operation. This procedure is for a single UPS without an external bypass panel.
Step 1: Set the input Q1 switch to On
Step 2: Wait until the end of the UPS initialization with PFC start-up.
Step 2: Push the Menu Button
Step 3: Scroll to “Maintenance”
Step 4: Choose “Start the UPS”
Step 5: Turn the Q4S Switch to On
Step 6: Turn the output switch Q5N to On
Step 7: Turn the maintenance bypass switch Q3BP to Off
Step 8: Set the battery circuit breaker(s) QF1 to the On Position.
Step 9: Press the Green “Inverter Start Button”
The Inverter Assumes the load, and the UPS is normal operation with the load protected.
Caution: Never remove any covers or panels. There are no user serviceable parts inside.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.