Browse FAQs



What is the difference between an InRow RP, InRow RD (600mm), and InRow RC (600mm)?
The minimum required kW for 1 direct expansion unit is 12kw and 12kw for chilled water . There should also be a consideration regarding humidity control.
What are your humidifier specifications and control operations for the InRow RP?
... between the humidify setpoint and the average return air humidity of all the units in the cooling group (if more than one unit is ...
UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... , g50 AV Units , Smart- ... acrc301h, acrc301s Cooling Units , ... ap9320 Environmental Monitoring Units FM35XX Network Air , acda901, ... acrc ACRCXXXX InRow Chilled Water (except ACRC3XXX ... ... your local APC Cooling Support team) ... ... ACRP5XX, ACRD5XX InRow RC, RP , RD AOS ... ... your local APC Cooling Support team) acsc ACSC1XX InRow SC AOS v ... ... your local APC Cooling Support team) raru ACFXXX Rack Air Removal Unit AOS v3 ... ACRD1XX, ACRD2XX InRow RD AOS v ... (via your local APC Cooling Support team) nb200 NetBotz 200 Rack Monitor (nbrk0201)
ACSC1XX Spare Parts List
This document contains the Spare Parts List for ACSC1XX units . ... Please contact Cooling Tech Support to confirm the part numbers before quoting as some may have changed. ... Manufacturing # ... CONDENSATE PUMP WIRE ASSY CP JUMPER (for activation without the water sensor kit) ... FITTING 1/8" BARB TEE (for air differential pressure switch) ... Front Door Assembly - Spare Part ... InRow RC/SC Filter 1/2" Washable - Spare Part (default) ... Wire Assembly Base
APC Schneider Cooling Unit Identification
APC Cooling Unit identification. All Cooling Units . APC Unit Identification FM Air / Water /Glycol Air Pattern W= Water Cooled F= Water Cooled D= Water Cooled ... G= Glycol Cooled ... B= Glycol Cooled ... P= Glycol Cooled ... W= Hot Water Air Pattern ... coil C= Chilled Water Air Pattern C= Chilled Water Air Pattern ... Main C= Chilled Water Air Pattern W= Water Cooled ... G= Glycol Cooled BA=208 ... Air Pattern W= Water Cooled ... G= Glycol Cooled Air Pattern W= Water Cooled
Inrow Chilled Water Units Internal Volumes
Issue: Inrow Chilled Water Units Internal Volumes
Why is my ACRP excessively cycling?
Data Center Cooling The InRow RP works to prevent ... ... load that the RP is given. ... With the supply air and cool setpoints both at ... In the Inrow configuration, the supply air setpoint controls the temperature of the air the unit supplies to the ... The cool setpoint controls the ... ... relative to the cool setpoint). Setting the cool setpoint between 72 ... and monitoring the unit performance, adjusting the cool and supply air setpoints as needed ... ... will enable the unit to use the ... under "configure unit " on the ... interface under the unit tab, then ...
What are the minimum load requirements for the ACRP DX?
InRow Cooling ... The InRow RP continually adjusts its cooling output to accommodate varying loads. The cooling output is determined by the difference between the supply air temperature setpoint and the actual supply air temperature as well as the airflow (for each of the cooling units in the cooling group if more than one cooling unit is present). ... At its lowest speed, the equipment cooling capacity is approximately 10 kW but is is recommended to have at least 13 to 15 KW of load per unit .
Where can I get support for APC and MGE Products?
Assessment Services Auto and Air Inverters ... Battery Replacement Services ... Data Center Facility Cooling - Andover Continuum or TAC Vista ... EcoBreeze Air Economizers ... Environmental Monitoring Unit ... High-Density Cooling Enclosures ... InRow Chilled Water InRow Direct Expansion InRow Pumped Refrigerant Installation Services ... MGE Service Bypass ... Network Integration Services ... On Site Service ... Portable Cooling ... Power Distribution Units ... Project Management Services ... Remote Monitoring Services ... Room Cooling Accessories ... Row Cooling Accessories ... Service Bypass Panel Service Plans ... Start-Up Service Stationary Power Distribution Units ... Training Services ... Uniflair Chilled Water


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.