Browse FAQs



Data Center Expert | How do hardware and software support contracts work?
StruxureWare Data Center Expert Appliances can have hardware warranty up to a total of 5 years , which includes 2 years of factory warranty.
Data Center Expert | Why does StruxureWare not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert (DCE) ... StruxureWare Central (SWC ... StruxureWare Data Center Expert (all versions ... StruxureWare Central (all ... SturuxureWare Data Center Expert requires a 64 ... passcode and the Data Center Expert's MAC address. StruxureWare Data Center Expert (DCE) ... ... to gather specific information about the alert ... 3 . If you ... 5 . To add ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine
Data Center Expert | How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
... Upon launching the StruxureWare Data Center Expert client an error ... StruxureWare Data Center Expert (DCE) ... StruxureWare Central (SWC ... StruxureWare Client (potentially ... StruxureWare may be attempting ... ... Installation directory for StruxureWare Data Center Expert . (default ... C:\ Program Files (x86)\ StruxureWare Data Center Expert X.X ... 3 ) Within the ... -vm "C:\ Program Files (x86)\ StruxureWare Data Center Expert 7.2.7\dcexpert\jre\bin\javaw.exe" 5 ) Save the file and open the client.
Video: Data Center Operation | Copying files from the StruxureWare Data Center Operation
How to copy files from the StruxureWare Data Center Operation ... StruxureWare Data Center Operation ... StruxureWare Data Center Operation (All Versions) ... In this document, we will be using a free program called WinSCP. You can find this program . ... 1. Open the application ... 3 . Enter log in credentials in both "Username" and "Password" fields ... 5 . Using the "Arrow up button" to navigate up a directory, continue click the icon until the directory window reads / ... 1. Double click on data folder ... 3 . Locate the backup to save off server
Battery Age and UPS Age shown incorrectly in StruxureWare Data Center Expert.
Battery Age and UPS Age shown incorrectly in StruxureWare Data Center Expert . ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert 7.x ... Battery Age and UPS Age can have 5 different date formats on newer firmware. ... 3 : mmm-dd-yy ... StruxureWare DCE may not show these formats correctly. ... file should be extracted and added to StruxureWare DCE.
Video: How do I change the temperature units within the StruxureWare Data Center Expert Client?
... units within the StruxureWare Data Center Expert Client? StruxureWare Data Center Expert StruxureWare Central StruxureWare Data Center Expert all versions The StruxureWare Data Center Expert client temperature units ... The StruxureWare Data Center Expert client temperature units ... 1. Close the current session of the Data Center Expert client ... 3 . Click on "Control Panel" ... 5 . Click on the "Formats" tab ... 8. Reopen your Data Center Expert client ... 1. Close the current session of the Data Center Expert client ... 3 . Click on "Control Panel" ... 5 . Click on the "Formats" tab ... 8. Reopen your Data Center Expert client
How to change a RAID battery on the StruxureWare Data Center Expert Enterprise server?
... battery on the StruxureWare Data Center Expert Enterprise server? StruxureWare Data Center Expert StruxureWare Central StruxureWare Data Center Expert all versions ... configuration of the StruxureWare Data Center Expert Enterprise server is ... ... a Raid- 5 configuration that has ... This battery is crucial for high data integrity. ... See Figure 3 -1. ... 3 With the cable oriented toward the back, angle the left side of the RAID battery into the left side of the battery bay. ... 5 If not already done, route the battery cable through the right chassis wall.
Video: How do I retrieve surveillance clips in StruxureWare Data Center Expert
Retrieving surveillance clips in StruxureWare Data Center Expert . ... StruxureWare Data Center Expert (DCE) ... StruxureWare Data Center Expert (DCE) ... 3 ) Within the Thumbnails pane, you will see the camera thumbnails for your NetBotz Appliances that are in the group you selected. ... 5 ) Within the Choose Date section, select either Relative or Date Range.
Can StruxureWare Data Center Expert output a 32 bit register with its Modbus output?
... single register in StruxureWare Data Center Expert's modbus output is ... StruxureWare Central / StruxureWare Data center Expert StruxureWare Central any version StruxureWare Data center Expert any version ... single register for StruxureWare is a 16 ... ... as 6553. 5 . ... bit register in StruxureWare . ... this limitation, StruxureWare Data Center Expert can be configured ... StruxureWare does not know ... This is also why this should be done upon initial setup as if the system is already configured and a register is changed, the polling software must be reconfigured with the new registers. ... This math must all done on the side of the querying application .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.