Technical FAQs

Ask a Question

End of Support Announcement for WallBotz 300, 300B and RackBotz 300 and 303

Issue:

End of Support Announcement for WallBotz 300, 300B and RackBotz 300 and 303

Product Line:

NetBotz

Environment:

NetBotz version 1 WallBotz 300, 300B and RackBotz 300 and 303

Cause:
End of Life, End of Support

Resolution:

End of Support Announcement for WallBotz 300, 300B and RackBotz 300 and 303

The following NetBotz products will reach the end of their support life on January 31, 2005:
WallBotz 300B
WallBotz 300
RackBotz 303
RackBotz 300

After that date, NetBotz may not take support calls or E-mails regarding these products. NetBotz also may not issue any further software releases or patches for these products after that date. 

Please note that the Rack and wall versions of the 310 and 400 units are also end of support
Was this helpful?
What can we do to improve the information ?