General functions of a MicroAC control platform DG3
Published date:
11 June 2020
Issue:
General functions of a MicroAC control platform
Product line:
Airflow
Environment:
Data Center Cooling
Cause:
Resolution:
The MicroAC is an electronic control for the complete management of precision air-conditioners, both in direct expansion versions (with 1 or 2 compressors), with 1 or 2 heating elements or with batteries (valve on the heating battery and/or valve on the cooling battery). The control also allows the management of a humidifier (with CDA type control or Humicontrol) and dehumidification with various pre-settable configurations. In addition, it can also be used in precision units for "Shelters" with management of the condenser fan.