Browse FAQs



How do I replace a single phase Symmetra battery module?
Remove the front cover of the UPS or XR frame and locate the faulty battery module(s).
Single Phase Symmetra XR Frame Compatibility
Symmetra RM UPS : SYRMXR4B4.
How to change the Input Voltage Select Jumper on a Symmetra Power Array
... environment of my Symmetra Power Array and ... Symmetra Power Array Before the UPS is started up, an ... : UPS must be completely ... 1 . Switch the ... ... front of the UPS . 3. Open and lockout the circuit breaker for the circuit that feeds the UPS . 4. Remove all battery modules from the UPS . 5. Disconnect any extended run ( XR ) battery frames from the UPS . ... 1 . Refer to figure below. Remove the screw that secures the voltage select access panel to the frame . ... 3. Replace the voltage select access panel and continue with connecting the UPS to utility power.
Steps to take when moving a Symmetra Power Array from one location to another
When you first receive your Symmetra Power Array, ... in the " Symmetra User's Manual" ... Unpacking and Installing Frame ) to hold ... on moving your UPS in the future ...
E3 error message on the Symmetra Extended Run Battery Frame (XR frame)
The XR frame of a single phase Symmetra displays E3 ... mainframe indicates an XR Frame Fault. Symmetra Power Array Symmetra RM Symmetra LX ... message on the Symmetra XR Frame is an indication ... communication between the Symmetra mainframe and the Symmetra Extended Run ( XR ) Battery Frame . ... located in the XR Frame . ... function of the UPS if it were ... ... that event the UPS goes on battery ... the Extended Run Frame . ... the Extended Run Frame will alleviate this ... ... card on the Symmetra Extended Run Frame :
Video: How do I properly reset a Symmetra XR Frame Communications Card (SYXRCC or SYAFSU16)?
Symmetra Power Array Symmetra RM Symmetra LX The XR frame shows a fault ... related to the XR frame . ... card on the Symmetra Extended Run Frame . 1 ) Disconnect the ... back of the Symmetra Extended Run Battery Frame and wait for ... ... being held by one of the thumbscrews ... ... 60 seconds the UPS will re recognize ... the Extended Run Frame . The following video demonstrates the procedure of reseating and installing the Symmetra XR Communications Card:
Batteries discharged to a low voltage in a single phase Symmetra frame
Single phase Symmetra battery modules are ... Symmetra Power Array Symmetra RM Symmetra LX 1 .) If ... ... to place the UPS into a bypass ... ... installed in a Symmetra frame , it must ... If the Symmetra is powered down ... installed in the frame , they will ... ... to place the UPS into a bypass ... All Symmetra and Symmetra RM units ship ... : Symmetra LX was designed ... ... only applies to Symmetra Power Array and Symmetra RM. The Symmetra will not be ... ... modules in connected XR frames).
What is the proper way to place a single phase Symmetra UPS into maintenance bypass?
... to place a Single -Phase Symmetra UPS into maintenance bypass ... Symmetra Power Array Symmetra RM Symmetra LX Single phase Symmetra UPS systems feature a ... ... state for a single phase Symmetra UPS system. ... bypass on a Single -Phase Symmetra UPS is to first command the UPS to bypass before ... 1 . From the ... " / " UPS into Bypass" ... There is still power present inside the Symmetra frame . ... If work is to be performed inside the frame , it needs to be done by APC's Field Service Engineers when the UPS is fully powered down.
Input Circuit Breaker Requirements for Symmetra PX 20/40/80 kw
This document describes the required input over current protection (circuit breaker) required when installing a Symmetra PX ... Symmetra PX1 Products ... Input Circuit Breaker Requirements for Symmetra PX 20/40/ 80 kw ... ISX 20k (All-in- One ) ... Symmetra PX 40 ... Symmetra PX 80 ... (APC Symmetra PX Frame Installation Deviation and Selection of Input Circuit Breaker Ratings)
What is the maximum number of XR frames allowed with a Symmetra PX 20, 40 and 80kw solution?
Symmetra PX; What ... maximum number of XR frames allowed with a Symmetra PX solution? Symmetra PX 20, ... ... maximum number of XR frames allowed with a Symmetra PX solution is ... ... size of the Symmetra PX Main Frame . For a Symmetra PX 20 or 40kw Frame , the maximum ... Battery Frames) XR frames. ... a runtime of 1 hr 40 mins ... ... of addresses for XR frames. ... a fully populated XR frame is SYCFXR8- ... ... consists of the XR frame with 8 Batteries ... ... this equals an XR frame with 32 Battery ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.