Browse FAQs



Does the CCS Injection OpenSSL vulnerability (CVE-2014-0224) affect APC products?
Schneider Electrics' Data Center Business has conducted a vulnerability assessment on the following platforms and found current shipping versions of each are not affected by the aforementioned vulnerabilities. ... PowerChute Network Shutdown versions 3.1 and 4 .0 Appliance for VMware utilizes v0.9.8e. ... Regular vulnerability assessment and further investigation is ongoing on other Schneider Electric platforms in addition to the above and will be detailed if discovered.
Are StruxureWare DCE or NetBotz vulnerable to CVE-2017-7494 (Samba related vulnerability)?
NetBotz (botzware) v 4 .X ... NetBotz 4 .X is not vulnerable to this issue because an unaffected version of Samba is used. ... Regular vulnerability assessment and further investigation is ongoing on other Schneider Electric platforms in addition to the above and will be detailed if discovered.
Are StruxureWare DCE or NetBotz products vulnerable to Stack Clash (CVE-2017-1000364 and related IDs)?
NetBotz (botzware) v 4 .X ... NetBotz 4 .X is not vulnerable to this issue because NetBotz doesn’t use glibc and it also doesn’t use a kernel that is vulnerable. ... Regular vulnerability assessment and further investigation is ongoing on other Schneider Electric platforms in addition to the above and will be detailed if discovered.
Are StruxureWare DCE or NetBotz vulnerable to CVE-2016-5195 (Dirty COW Vulnerability)?
NetBotz (botzware) 4 .x ... Regular vulnerability assessment and further investigation is ongoing on other Schneider Electric platforms in addition to the above and will be detailed if discovered.
EcoBreeze Variable Speed Drive Technical Spec’s
immunity test conforming to IEC 61000- 4 - 4 level 4 Electrostatic discharge immunity test conforming to IEC 61000- 4 -2 level ...
Galaxy VX; What is the Airflow and BTU heat dissipation?
... the estimated airflow in m^3/hr and CFM for the same four load level (three at 30c and one at 40c ...
ISX-GEN-ATS; how do I recalibrate the ATS panels Generator fuel level?
... will briefly (for 4 seconds) display ... * CAL FUEL LEVEL TO xxxxx” ... of the fuel level sensor in tenths of ohms.
What is the Smart-UPS On-Line surge and spike test data?
Voltage Spikes IEC standard ( level ): IEC 61000- 4 - 4 (1000 volts)
Refrigerant charging table for a Uniflair Unit
4 . Wait for an hour and check vacuum level .
What are the causes of premature motor failure in single-phase motors?
In 2003 Franklin Electric SA lead four training courses throughout South Africa in an effort to increase the level of expertise in the borehole industry ...


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.