Can I deploy an EcoAisle system even if I don’t have all of my equipment install
... hot or cold aisle contiainment ... support 900, 1200 , 1500 and ... and 6ft) wide aisles . If one of these increments are not the right size, the panels can be easily modified to fit any aisle width between 900 and 1800mm. Blank Panels available for 300, 600, 700, and 750mm wide spaces • Options available to support (900mm, 1200mm, 1500mm , and 1800mm aisle widths ) • Panels Can also be modified in the field to fit odd aisle sizes • Safe Slide Doors support hot or cold aisles