Browse FAQs



DAC, Cancoil Installation Manual
... how to properly install a legacy DAC ... Install Air Cooled Condenser Installation and Operating Instructions DAC Air Cooled Condensers For information ... Cancoil air-cooled condensers have been ... ... equipment, proper installation and set- ... ... be used if air-cooled quipment is located ... Installation Date __ ... ... properly sized and installed to insure oil ... ... risers should be installed with a trap ... Cancoil air-cooled condensers are available ... variety of optional fan cycling controls, ... are shipped without fan controls. Check ... ... high affinity for water . ... amperage on the fan motor(s ...
Where can I get support for APC and MGE Products?
Air Cooled Chillers ... InRow Chilled Water ... Installation Services ... Outdoor Enclosures ... Software Installation ... Uniflair Chilled Water
APC Schneider Cooling Unit Identification
... FM Air/ Water /Glycol ... Expansion A= Air Cooled E= Air Cooled W= Water Cooled F= Water Cooled D= Water Cooled ... W= Hot Water ... C= Chilled Water ... C= Chilled Water ... C= Chilled Water ... Main A= Air Cooled W= Water Cooled ... ) A= Air Cooled W= Water Cooled ... ) A= Air Cooled W= Water Cooled ... ) A= Air Cooled E= Air Cooled w/Multicool R= Air Cooled w/Remote ... W= Water Cooled F= Water Cooled w/ ...
Refrigerant charging table for a Uniflair Unit
Install . Air-cooled DX units must ... to a remote outdoor condenser. ... Systems with remote outdoor condensers must have ... Install all refrigerant lines in accordance with applicable industry guidelines as well as local and national codes and regulations. ... • All refrigerant lines/chilled water piping are free from debris. ... • All refrigerant pipes are installed with proper supports and approved refrigerant line clamps. ... When brazing field- installed copper refrigeration lines, use a nitrogen purge to minimize ... Install a ball valve before the micron gauge to prevent damage to the micron gauge during charging.
What are the operational conditions for an InRoom (Stulz) Unit
Install Outdoor ambient conditions: ... Chilled water -/cooling water pipes: Maximum water head pressure: 10 bar (145 psi) Maximum equivalent length of piping between the cooling unit and the air cooled condenser: 60 m (200 ft) ... Entering water temperature (EWT) for CW coil: 7°C (44.6°F) Leaving water temperature (LWT) for CW coil: 12°C (53.6°F) ... Chilled water medium (CW): 0% Glycol
How does a chilled water actuator work on an acrc301h to control dew point after a power loss?
How does a chilled water actuator work on an acrc301h to control dew point after a power loss? ... Install , Repair. ... Upon restart, the fans start first to allow the sensors some time to recognize the air temperature and humidity as well as the fluid temperatures.
How to set points and sensor offsets on a Uniflair High Capacity unit with Touch Screen Display
Install . ... • Circuit Entering Chilled Water Temperature Sensor Offset: - ... • Circuit Leaving Chilled Water Temperature Sensor Offset: ... Outdoor Temperature Sensor Offset: Delta ... • Hot Water (Reheat) Temperature Sensor Offset: Delta
Network Air FM unit spare parts list
Install ... 875-4183 Glycol/ Water LL ... 875-4182 Glycol/ Water & Air LL ... HEAT EXCHANGER - FM NAM 35KW WATER , R22 ... HEAT EXCHANGER - FM NAM 40kw WATER , R22 ... HEAT EXCHANGER - FM NAM 50kw WATER , R22 ... Indoor Receiver Relief Valve 425psig 3/8 MPT X 1/2 FLARE (for outdoor unit) ... Rope Water Detector Assembly (0w1586 cable only) ... Spot Water Detector (Assy. ... Water Flow Switch Assy
How to navigate through an Network Air FM unit display
... identify the hardware installed in this System ... ... the coil configuration installed in the Modules ... ... ® (chilled water ) and DX ... ... (PCIOMs) installed in the user ... Installation ... of air filters installed in the Modules ... ... recommended for typical installations . Water ... DX 60 Hz Installation ... and humidity probes installed must be supported ... ... (glycol or water ) flow to ... ... flow switch is installed : ... —for the water or glycol line ... ... for the chilled water input to the ... coil or chilled water coil (Systems using chilled water only).
How to clean Heatcraft-Larkin Refrigeration condensers
Install , Repair ... Air cooled condensing units require a minimum of maintenance. ... All of the condenser fan motors have sealed ball bearings. ... Reference Heatcraft-Larkin Refrigeration Products Remote Air Cooled Condensers Manual. Bulletin H-IM-73A June 2000 Part Number 90800801


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.