Browse FAQs



Data Center Expert | How do hardware and software support contracts work?
Product Line: StruxureWare Data Center Expert (DCE)
Why does StruxureWare Data Center Expert not accept my One Time passcode?
StruxureWare Data Center Expert is not accepting ... StruxureWare Data Center Expert StruxureWare Central / Data Center Expert all versions. SturuxureWare Data Center Expert requires a 64 ... passcode and the Data Center Expert's MAC address. 1 . In a ... AP9465 = StruxureWare Data Center Expert Basic ap9470 = StruxureWare Data Center Expert Standard AP9475 = StruxureWare Data Center Expert Enterprise AP94VMACT = StruxureWare Data Center Expert Virtual Machine SFDCOBASE = StruxureWare Data Center Operation ... a VM or Data Center Operation. ... all the relevant information . ... a word processing application such as notepad ... ... . Launch your Expert client.
StruxureWare Data Center Expert v7.4.2 is no longer available
Resolution You must have a valid support contract to receive the software update.
How can I resolve “Failed to create java virtual machine.” error when launching StruxureWare Data Center Expert client?
1 ) Navigate to ... Installation directory for StruxureWare Data Center Expert . (default ... C:\ Program Files (x86)\ StruxureWare Data Center Expert X.X ...
Data Center Operation | Video: Copying files from the StruxureWare Data Center Operation
1 . Open the application 2. Enter IP address or hostname within the "Host Name" field
Restoring StruxureWare Data Center Expert backup to a new Virtual Machine causes system to not fully boot up.
Restoring StruxureWare Data Center Expert backup to a ... StruxureWare Data Center Expert StruxureWare Data Center Expert Virtual Machine ( ... Migrating a StruxureWare Data Center Expert hardware server to ... ... equivalents for the StruxureWare Data Center Expert Basic , Standard, ... ... , and the StruxureWare Data Center Expert virtual appliance will ... 1 . Gracefully shut down the virtual appliance. ... See StruxureWare Data Center Expert virtual server equivalent configurations. ... Changes in the disk space will take effect once the StruxureWare Data Center Expert virtual appliance has restarted. ... To store large amounts of surveillance data , using a remote repository is recommended.
Why isn't my DNS change saving in StruxureWare Data Center Expert?
Changing DNS entries in StruxureWare Data Center Expert UI for VM does not save changes. ... StruxureWare Data Center Expert ... StruxureWare Data Center Expert VM with single NIC configured ... It has been seen where changing a DNS entry in StruxureWare Data Center Expert (DCE) when using the console application does not cause the system to reboot and save the DNS changes. This only happens on a system with a single NIC so it is not seen on the DCE hardware servers, only on a DCE VM server.
Can StruxureWare Data Center Expert output a 32 bit register with its Modbus output?
A single register in StruxureWare Data Center Expert's modbus output is ... StruxureWare Central / StruxureWare Data center Expert StruxureWare Central any version StruxureWare Data center Expert any version ... output of a single register for StruxureWare is a 16 ... ... handled by a single register. ... bit register in StruxureWare . ... this limitation, StruxureWare Data Center Expert can be configured ... StruxureWare does not know ... ... value of either 1 or 2. ... ... , the polling software must be reconfigured ... 31000 returns 0000000000000001 If this were a single register, = 1 ... This math must all done on the side of the querying application .
What type of information is provided in an SNMP trap from StruxureWare Data Center Expert?
... What type of information is provided in ... SNMP trap from StruxureWare Data Center Expert ? StruxureWare Central / Data Center Expert StruxureWare Central any version StruxureWare Data Center Expert any version StruxureWare has the ability ... ... from our APC software downloads page. ... be version related info as well so ... ... clearing traps for StruxureWare are based on ... The traps also provide additional information / arguments as described in the mib: ... - The first argument is the unique ISXC alarm ID. ... - The fourth argument is the unique ISXC device ID. ... - The thirteenth argument is the unique ISXC sensor ID.
Data Center Expert | How do I upgrade my appliance version?
Process for upgrading StruxureWare Data Center Expert . ... StruxureWare Data Center Expert (DCE) - Basic Appliance (AP9465) ... StruxureWare Data Center Expert (all versions) ... You must have a valid currently active software support contract to recieve upgrade files. ... 1 ) Extract the downloaded upgrade zip file. ... Upgrades usually take an hour or less to complete, but for certain upgrades it may take significantly longer depending on the number of devices and amount of historical data .


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.