Browse FAQs



How do I connect a EPO (Emergency Power Off ) circuit to Galaxy VM?
... ) circuit to Galaxy VM ? Galaxy VM ... ) circuit to Galaxy VM ? When the UPS is EPO'd, ... There is also an option in the UPS Tuner (Schneider software) to have the UPS go to static bypass on EPO (default setting is no). ... Tripping of the upstream breaker could be a code requirement, typically if UPS is located in the data center. ... Note; in parallel systems, only the UPS in which the EPO is activated is affected; remaining UPS will still be powered.
Video: How to configure the display network settings on a Galaxy VM
Issue: Configuring Network Settings on Galaxy VM UPS Display
Video: Configuring output relays/input contacts on a Galaxy VM
Issue: Configuring Input Contacts & Output Relays on Galaxy VM UPS Display
Video: Changing the display Language, Date Format & Temperature Units on a Galaxy VM
Issue: Configuring Display Language, Date & Temperature Units on Galaxy VM UPS
How do I connect a EPO circuit to Smart-UPS VT or Galaxy 3500 Battery XR Frame?
How do I connect a EPO circuit to Smart- UPS VT or Galaxy 3500 Battery XR Frame? ... Smart- UPS VT & Galaxy 3500 Battery XR frames ... How do I connect a EPO circuit to Smart- UPS VT or Galaxy 3500 Battery XR Frame? ... This means that you shall connect UPS and XR in parallel by applying +24V on both connectors UPS j108 & XR j203, if you will EPO them both at same time. ... UPS can be configured in three other ways, concerning EPO. See UPS Installation manual for details.
How do I connect a EPO (Emergency Power Off) circuit to Galaxy VX?
... ) circuit to Galaxy VX? Galaxy VX ... ) circuit to Galaxy VX? ... A35JB8_R 1 _EN. ... When the UPS is EPO'd, ... There is also an option in the UPS Tuner ( ... software) to have the UPS go to static bypass on EPO (default setting is no). ... Tripping of the upstream breaker could be a code requirement, typically if UPS is located in the data center. ... Note; in parallel systems, only the UPS in which the EPO is activated is affected; remaining UPS will still be powered.
Where do I find an Operation Manual for Galaxy VM Series UPS?
Issue: Operation Manual for Galaxy VM Series


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.