Browse FAQs



UPDATED MARCH-2016: Unable to access my APC Network Management Card (NMC) enabled device via HTTPS (SSL/TLS)
... Network Management Card 1 (NMC1) ... ... Network Management Card 1 include (but ... ... who uses any one of the products ... One such example is ... ... future firmware update plans to address this ... ... Network Management Card 1 (NMC1) ... /100/ 160 kVA embedded UPS ... ... , RP, RD AOS v3 ... ... , ACRD2XX InRow RD AOS v3 ... ... a value of 1 to allow fallback ... Network Management Card 1 (NMC1) Information Bulletin: Effects of Microsoft Internet Explorer and other web browsers blocking key lengths less than 1024 bits​(blocking key lengths less than 1024 bits)
Maximum Size of SMS Message / Alert
The maximum size of an SMS text message sent via GSM is 160 single byte characters. Different carriers could potentially put lower limits.
Schneider Electric's Technical Support Policy for Older Versions of PowerChute Software
... far beyond this stated commitment, but this 1 - year policy is stated here so customers may take it into account for planning purposes ...
Spare parts list for ACRD1XX, and ACRD2XX
1 /2" ODF - SPARE PART 0.265 160 .0 160 .0 160 .0 0.102 70. ...
Single Phase Symmetra Extended Run (XR) Frame Cable Lengths
This information can be relevant if a user is planning on installing the products in slightly different areas - different racks, for example.
Steps to take when moving a Symmetra Power Array from one location to another
... case you need to either send any components back to the APC or if you plan on moving your UPS in the future.
How to adjust the lens on the NetBotz Wallmount or the Camera Pod 160?
To adjust the focus and field of view settings: 1 . Loosen the adjustment screw by turning it counter-clockwise.
3 Phase Products Service Level Agreements; Definition of coverage as relates to the service level agreements offered by SE
UPS & PDU Advantage Plus: See attached file; ARUO-ACQK4F_R7_EN_ Advantage Plus ... 1 Annual PM Visit ... UPS & PDU Advantage Prime : See attached file; ARUO-ACQGSD_R7_EN_ Advantage Prime ... 1 Annual Preventive Maintenance Visit ... UPS & PDU Advantage Ultra: See attached file; ARUO-ACQFVH_R6_EN_ Advantage Ultra ... 1 Annual Preventive Maintenance Visit 1 Set of air filters if applicable
Problem: PowerChute Network Shutdown does not turn off the UPS following a shutdown event.
... of the PowerChute service , e. ... To make sure the UPS turns off as planned when a shutdown event occurs, PowerChute shutdown events should be configured with a delay of 120 seconds. ... This issue also applies to the Advanced Configuration option in Multiple Mode which, in a Multiple configuration, enables you to turn off one UPS when it goes on battery.
ProtectNet surge performance ratings
1 ,500 Vrms 8 Vdc 1 ,800 Vrms < 50 Vpk < 1 ,700 Vpk 6,900 A ... 1 ,500 Vrms 8 Vdc 1 ,800 Vrms < 50 Vpk < 1 ,700 Vpk 6,900 A ... 1 ,500 Vrms 60 Vdc 1 ,800 Vrms < 50 Vpk ... 1 ,500 Vrms 8 Vdc 1 ,800 Vrms < 50 Vpk < 1 ,700 Vpk 6,900 A ... <60vpk 250a (8/20us) 250a (8/20us)


Results 1 - 10 of 50

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.