{}

Our Brands

{"support":{"yesButton":"Yes","noButton":"No","feedback":{"title":"What can we do to improve?"},"submitButton":"Submit","successMessage":"Thank you for your feedback","title":"Did this answer your question?","feedbackPercentLabel":"of people found this helpful","captcha":{"error":"Please check the box"}}}

Search FAQs

{"searchBar":{"inputPlaceholder":"Search by keyword or ask a question","searchBtn":"Search","error":"Please enter a keyword to search"}}

Netbotz 500, 420, or 320 loses configuration when it is rebooted.

Issue:

Netbotz 500, 420, or 320 loses configuration when it is rebooted

Product Line:

NetBotz

Environment:

Version 2 NetBotz

Cause:

Due to a change on the Netbotz devices, some 500s, 420s, and 320s made in mid 2007 began losing some configuration when the system was rebooted. Prior to rebooting the device, the unit would function normally.

Resolution:

Version 2.6.2 of Botzware has fixed this issue.

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.

Can't find what you are looking for?

Reach out to our Customer Care team to receive information on technical support, assistance for complaints and more.