Installing NetBotz 5.x firmware after a failed install will cause the 2nd install to get stuck
Published date:
09 February 2021
Issue:
Installing Botzware 5.x after a failed install will cause the 2nd install to get stuck
Product Line:
NetBotz
Environment:
NBRK0750 NBWL0755
Cause:
It's been seen where trying to reinstall the current firmware on a NetBotz 75x unit can cause an exception. Trying to reinstall again will cause the NetBotz to become unresponsive.
Resolution:
Simply power cycling the device should allow the unit to fully boot back to the original firmware.
Please note that this may happen with any failed upgrade.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.