What kind of microphone can I use on a NetBotz appliance / Camera pod 160?
Published date:
14 May 2020
Issue:
What kind of microphone can I use on a NetBotz appliance / Camera pod 160?
Product Line:
NetBotz
Environment:
NetBotz version 3 appliances (NBRK0355, NBRK0455, NBPD0160)
Cause:
NetBotz appliances and / or Camera pods are capable of using external microphones.
Resolution:
The proper microphone to connect to a NetBotz is a stereo dynamic (non condenser) microphone with a 3.5 mm jack. It is advised that you do not use a directional or "shotgun" microphone.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.