Technical FAQs

Ask a Question

Can the load ratings of NetShelter SX cabinets be exceeded? Is there a cabinet with a higher load rating than the NetShelter SX?

Issue:
Customers question if the stated load rating of a cabinet can be exceeded, and if so by how much. Is there any "wiggle room" in the load ratings? 

Product Line:


Environment:
All versions and serial ranges.

Cause:
A customer has an application whose load rating is beyond that of the NetShelter SX stated load rating. 

Resolution:

The NetShelter load ratings are not to be exceeded. There is no "wiggle room" in the load ratings. 
All stated load ratings include only the weight of the equipment installed into the cabinet. The stated load ratings do not include the weight of the cabinet, pallet or packaging. 
For applications whose load ratings exceed those of the NetShelter SX there’s a new NetShelter cabinet with a higher load rating; the NetShelter SX3K: https://www.apc.com/shop/us/en/categories/racks-and-accessories/racks-and-enclosures/integrator-ready-racks/N-1yeks2t
The NetShelter SX3K cabinets have both Shipping Load and Dynamic Load ratings of 3500 lbs., and a Static Load rating of 4250 lbs. 
 
Was this helpful?
What can we do to improve the information ?