Technical FAQs

Ask a Question

Can the side doors or rear fan panels of the NetShelter CX/CX2 be secured with the NetBotz HID door handle? If not, is there a more secure option?

Issue: 
I customer is looking to make the side door more secure, thus making access to the rear fan panels more secure. 

Product Line:
NetShelter CX
 
Environment:
All models and serial ranges. 
 
Cause:
The customer cannot find options to make the rear fan trays more secure. 
 
Resolution:

Currently there is no way to increase security to accessing the rear fan units or side doors. The HID door handle solution available for the front door cannot be implimented on the side or rear. 
 
Was this helpful?
What can we do to improve the information ?