Browse FAQs

SmartConnect Portal indicates that the firmware is out of date on my SmartConnect enabled UPS. How do I update it?

Published date: 01 April 2021


Issue:

SmartConnect Portal indicates that the firmware is out of date on my SmartConnect enabled (EcoStruxure™ Ready) Smart-UPS


Product Line:

Smart-UPS

Environment:

EcoStruxure™ Ready Smart-UPS models with the prefix SMT, SMC, SMTL, SCL, and SMX, that have a SmartConnect Ethernet port.
All Serial Numbers

Cause:

EcoStruxure™ Ready Smart-UPS products are able to download the latest UPS Firmware from the Cloud.

Resolution:

1 - To upgrade the firmware you can do so via the cloud portal. See the instruction here https://www.smartconnect-support.apc.com/help/EN/index.html#page/EcoStruxure%2520Ready%2520Smart-UPS%2520Help%2520Center%2FMN04.6.2.html%23

2 - The other option for upgrading the firmware is Via the "Configuration" menu on the UPS LCD screen. You can update the UPS firmware by selecting "​Install FW?"
Note: This option will only be seen once a Firmware Image has been automatically downloaded by the UPS from the cloud. 

Once you select "Install FW?" your options are:
• Next off (Updates the UPS Firmware next time that the UPS is turned off)
• Now (Updates the UPS firmware immediately without interrupting operations)
• Don't Install

The update will take approximately 5 minutes to complete from the time you initiate the update. You may not have battery back up available during some of this time. If you have a high profile application you may want to use "Next Off" so that the UPS updates itself the next time you reboot the unit rather than doing the upgrade live.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.