NetBotz Room Monitor 355/455 | POE Power Specifications
Published date:
21 July 2020
Issue:
NetBotz Room Monitor 355/455 POE Power Specifications
Product Line:
NetBotz
Environment:
NetBotz Version 3 using POE
Cause:
POE specifications
Resolution:
The NetBotz 355 and 455 are Class 0 POE devices.
The IEEE standard 802.3 for supplying power over Ethernet allows the device providing power to use a voltage between 36–57 V DC. The nominal voltage is 48 V with a current of 10–400 mA, subject to a maximum load power of 15.40 Watts.
Can't find what you are looking for?
Reach out to our customer care team to receive information on technical support, assistance for complaints and more.