Technical FAQs

Ask a Question

Dew Point Calculations on the NetBotz Appliances

Issue:

Dew-Point Calculations on the NetBotz Appliances

Product Line:

NetBotz

Environment:

NetBotz version 1 and 2

Cause:

Definition: Dew Point is the temperature at which condensations forms

Resolution:

When air comes in contact with a surface that is at or below its Dew Point temperature, condensation will form on that surface.

The following external site explains how the dew point is calculated: http://www.dpcalc.org/
 
Was this helpful?
What can we do to improve the information ?